Cancel
Showing results for 
Search instead for 
Did you mean: 

Line Item Properties

Experimenter
Experimenter

What are the best practises in setting item level user defined fields? Working to better organize tracking and managemen of line items.

 

Thanks

3 REPLIES 3

Re: Line Item Properties

Experimenter
Experimenter

We're looking to better address how the engineer manages the individual line items within a project.....

Re: Line Item Properties

Siemens Genius Siemens Genius
Siemens Genius

I think this is something realy cutomer specific.

 

It depends what kind of information you want to query for in regard of information reuse.

e.g. you store a specific number from your plm system visible into a udf to be able to find this specific line item for reuse or modify. ... or you want to create reports based on some informations in your line items ... in that case you can store them also into the udf's and reuse them for some queries. ... Or an ordernumber which comes from a diffrent system but has to be published to better find this lineitem to work on it. (if more departments work with the same line item)

 

BR

Christian

Re: Line Item Properties

Valued Contributor
Valued Contributor

I believe the UDFs do show up as properties on top-level (or you might have to create similar named properties) but it is possible to assign a value to a UDF property at run time and you will notice that the lineitem now shows that updated value. Typically, UDF values can be used for summary information like cost, price or a general status of the model associated with that lineitem (other than the basic status provided by base Rulestream).

 

Dharmesh