cancel
Showing results for 
Search instead for 
Did you mean: 

Multiple instances of different PartFamily in one grid

Experimenter
Experimenter

Please tell me, how to display multiple instances of different PartFamily in one grid.

For example, I have a part family called "Power transformer" which has properties "Length", "Width" and "Height" and part family called "Cabinet" which is also has these properties. 

How can i see all measurements of power transformers and cabinets in single grid? Is this possible?

 

My first thought was to create another part family - "Measurement", create a connection for it and populate it within a formula. In my Custom.vb file i created a method, which returns a collection of objects, containing these properties, but unfortunately, it's not working. Maybe there is a way to cast object to specific Rulestream.Kernel.Part?

2 REPLIES

Re: Multiple instances of different PartFamily in one grid

Genius
Genius

No special tricks required. Just specify the valid part families and you can add them.

 

grid.JPGvalid.JPG

Highlighted

Re: Multiple instances of different PartFamily in one grid

Experimenter
Experimenter

It works!

Thank you, Yuri