Cancel
Showing results for 
Search instead for 
Did you mean: 

Rebuild Solid Edge assembly

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hello!

I have a problem with assembly rebuild in SE.

I change the parameter one of the blocks in Rulestream Engineer and press the button "Rebuild Solid Edge".

SE does not receive parameters and geometry is not rebuilt.

 

Log file is written:

ERROR "COM object that has been separated from its underlying RCW cannot be used"

Log file in attch.

 

What could be the problem?

1 REPLY 1

Re: Rebuild Solid Edge assembly

Builder
Builder

Hi,

 

Can you provide more details on what you are trying?

If possible  can you provide following details:

1. Parts and Steps

2. Solid Edge version you are working on.

 

The error you mention looks like Solid Edge Internal error when trying to execute something in code.

 

Note : I think it is better to log an IR so it can be handled in better way.

 

Thanks,

OnkarP