Cancel
Showing results for 
Search instead for 
Did you mean: 

Removing properties window from Engineer UI for specific profiles

Experimenter
Experimenter

 

Is it possible to remove the propeties and tree model windows from the Engineer UI on specific profiles instead of the whole application?  I am in the process of trying to simplify the UI for a specific end user profile; rather than editing the top level process step, are there any profile settings that can be modified to hide those windows?

2 REPLIES

Betreff: Removing properties window from Engineer UI for specific profiles

Siemens Genius Siemens Genius
Siemens Genius

Of course this is possible,

Just put the people to a specific Role and attache this role to the Process

 

E.G.

Create a new process as copy

Create Process.png

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Then Uncheck Properties and Modeltree

Interface.png

 

And bind it to a specific role (e.g. Sales)

Profiles.png

 

That should do the trick Smiley Wink

Betreff: Removing properties window from Engineer UI for specific profiles

Valued Contributor
Valued Contributor

I am not too sure this will work for what was asked - this method just allows access to a given process to users in certain roles. But, ALL individuals in those roles will either see or not see those components based on the selection. If you truly want to show those components for some profiles and hide for others, the only way I can think of is to create a duplicate process and put the rest in a different role (not a good solution at all).

 

Dharmesh