Cancel
Showing results for 
Search instead for 
Did you mean: 

Rulestream Architect API

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi Experts,

 

Is there any API for Rulestream Architect (not Engineer) ?

If not, are there any plans for the future?

 

Thanks,

-Thilak Rao

7 REPLIES 7

Re: Rulestream Architect API

Valued Contributor
Valued Contributor
Why would you want an API of an API?

Re: Rulestream Architect API

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

To automate tasks in Architect.

Create applications, part family, its properties etc.

 

The uses are plenty.

 

-Thilak Rao

Re: Rulestream Architect API

Valued Contributor
Valued Contributor

I think there is no API but as far as I've noticed Architect is generally only a Client for Rules DB updates.

You can pretty easy check what DB activities are under Architect actions and then replicate them in your application.

You can run SQL Profiler on your rules DB, perform an action on architect and see what queries and in what order were executed on DB.

For creating PFs, properties etc. it's not a big deal to automate it using exactly the same queries as used by architect.

 

Adam Liszkiewicz
Configuratori Polska

Re: Rulestream Architect API

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

This is the approach I wanted to avoid. Typically no one guarentees the structure of the db schema and is subject to change without notice. But if the product has an API exposed then that is guarnteed to continue to work.

 

Thanks,

-Thilak Rao

Re: Rulestream Architect API

Valued Contributor
Valued Contributor

So I think you must wait for Siemens guys to expose any API...

 

Adam Liszkiewicz
Configuratori Polska

Re: Rulestream Architect API

Valued Contributor
Valued Contributor

RSArchitect is an application that runs stored procedures to both push and pull information in the Rules database. 

Re: Rulestream Architect API

Experimenter
Experimenter
Hello , will there be some description material or nuggets available in future for the stored procedures?

secondly, along with existing stored procedures to update /delete are there any stored procedures for creation(of applications, part families...)?


Thanks
Leelakumar