Cancel
Showing results for 
Search instead for 
Did you mean: 

Significance of NX additional attributes

Experimenter
Experimenter

What is the significance of various properties of  NX spec 'additional attributes' like  DocumentFile,DrawingFile,Working_file_name,Output_file_name,DocumentName.

1 REPLY 1

Re: Significance of NX additional attributes

Community Manager Community Manager
Community Manager

These are Meta Tags associated with the NX files, similar to right-clicking a file on your system, selecting properties and then going to the Details tab.  Rulestream is able to read and in some cases write to these attributes.  We recently made some updates to Solid Edge to allow for writing to some of these attributes.  I'm not sure of the status of the NX Additional Attributes so you'll want to test and see if they can be updated via Rulestream.