Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge on Windows 10 (1709)

Community Manager Community Manager
Community Manager

We've just been informed of the following issues with running Solid Edge on Windows 10, build 1709 ("Fall Creators Update").  This information is being provided for our SE Integration users.  Please contact your Solid Edge support team for more details.

 

Windows 10 1709 problems for SolidEdge

Several PRs have recently been filed against Solid Edge for issues that occurred after customers installed Windows 10 1709 (“Fall Creators Update.”)  The problems encountered were:

 

  • Performance issue when displaying menus. SE found that the performance of GetPixel was the culprit.
  • Display issue when dragging a dialog.
  • Change in behaviour during a drag operation.

 

The SE Team has filed a case with MS support for them to investigate these issues.

 

Microsoft has released a hotfix that addresses the GetPixel problem: https://support.microsoft.com/en-us/help/4058258/windows-10-update-kb4058258.