Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Disable Add-Delete-Copy choices in the right click menu in a grid.

Valued Contributor
Valued Contributor

And yes, I forgot to mention, that what you were trying to do with subpart is not possible (unless you want to use a dummy subpart) but can definitely be done with connection but you will need to handle the subpart creation (using your own button and corresponding code).

 

Dharmesh

Re: Disable Add-Delete-Copy choices in the right click menu in a grid.

Genius
Genius

Yes, I'm sure. Verified few times.

I have 2 grids on a UI step. One of them is mapped to the UIVoltages subpart collection the other one - to the UIVoltagesDisplay. The grids behave the same..

Highlighted

Re: Disable Add-Delete-Copy choices in the right click menu in a grid.

Valued Contributor
Valued Contributor

This is really odd - never seen this behavior. The grid context menu has always followed the user edit setting (if it was tied to a subpart) and disabled if it was tied to a connection. The next logical thing to do (you might have already tried it) is to see what happens when you click the 'add' while it is tied to a connection. Does it actually create a brand new part (under which subpart) and add it to a connection?

 

Dharmesh