Cancel
Showing results for 
Search instead for 
Did you mean: 

Using NX 11 assembly constraint "Distance" with distance limits

Experimenter
Experimenter

Hello,

 

Is there a way to apply the assemlby constrain "Distance" in Siemens NX11 wtih Rulestream, with distance limits?

 

For example, I have two 3D models with planes in the Part Navigator. I want to be able to position the models, so that they can move linearly in a range between two values, e.g. 10-100mm. Is there anyway to apply this constraint with Rulestream?

 

Thanks

3 REPLIES 3

Betreff: Using NX 11 assembly constraint "Distance" with distance limits

Siemens Genius Siemens Genius
Siemens Genius

Are they build up in an NX_Assembly Spec or will they be build up from scratch?

 

In the first case you have to find the offset and edit it (via Expression)

In the second case you can build it up with a offset (plane 2 plane)

Betreff: Using NX 11 assembly constraint "Distance" with distance limits

Experimenter
Experimenter

The assembly is built using a NX spec. The components that are positioned are retriever from teamcenter.

 

I know how to apply the constraints, e.g. distance, using planes. My question is if it is possible to make the distance constraint "dynamic" so that the components ends up in the closest point in that distance, e.g. 50-100mm,

Betreff: Using NX 11 assembly constraint "Distance" with distance limits

Siemens Genius Siemens Genius
Siemens Genius

Can you show an example for that?

Is it clear at which distance they have to be?

Can you measure this and use the value for placing them?