Cancel
Showing results for 
Search instead for 
Did you mean: 

Word Spec via Thin Client

Does anyone have any experience using the word spec via the Thin Client?  

If so does word need to be installed on the server? 

To generate the word document would I call g_RsEngineer.CreateOutput(PF.ObjId, Spec.SpecID, "", False)?

 

As described in this thread:

https://community.plm.automation.siemens.com/t5/Rulestream-Forum/Releasing-a-word-report-in-RS-Engin...

 

4 REPLIES

Re: Word Spec via Thin Client

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

It is not required to have Word installed on the server. The document will still be created correctly without it.

 

For Thin Client, we suggest using the Output tab on the Word Spec to create a PDF and then use the PDF Viewer Process Step to view it on a client machine.  Visiting the PDF Viewer Process Step will trigger the creation of the Word spec on the server.

 

Re: Word Spec via Thin Client

 

 

What needs to be done so my client is able to display the pdf?  I tried writing the pdf to the "C:\inetpub\wwwroot\ModelServicesWS\resource\file\output" but that did not work.PDf Viewer.png

 

 

 

 

Re: Word Spec via Thin Client

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

You just need to create the word spec in RS Architect and add a PDF output under the Output tab:

 

tc_word1.JPG

 

Then, create a PDF Viewer Process Step and point to this output:

 

tc_word2.JPG

  

At runtime, the word document and PDF will be created when you go to the PDF Viewer Process Step. They will be in the WIP folder in your working directory. If you save the line item, they will be saved to the .0000 folder in your working directory.

 

You will not need to use CreateOutput in this scenario but you will need to use custom.vb to move the files to the Release folder if required.

Re: Word Spec via Thin Client

That works but it's worth noting that the file name cannot have a space in it.