Cancel
Showing results for 
Search instead for 
Did you mean: 

Referencing Project and Line Item User-Defined Fields (UDFs) in a formula

Community Manager Community Manager
Community Manager

Project and Line Items may each have an unlimited number of user-defined fields (UDFs), however four to five UDFs each is a good practical limit. These UDFs are added through the System Administration tool.

 

To reference these UDFs, a property is created on the root part with the same name as the System Name of the desired UDF.  For example, a UDF named "Location" needs a corresponding read-only property on the root part named "Location".

 

Whenever the model is loaded, the Rulestream properties assigned to the Project/Line Item UDF fields (if they exist) will be initialized with the existing UDF values. 

 

An alternate method to reference a Project UDF or Line Item UDF without placing a property on the top part of the application is to use the following syntax:

 

   Me.Properties("UDFName").Value

 

By design, Project UDFs cannot be modified while editing a model - only Line Item UDFs can be modified. 

 

Setting a UDF Value

 

  1. Create a LineItem UDF named “myLIudf3”  (Architect’s Tools > System Administration menu, Line Item UDFs choice)
  2. Now create a property that contains the following formula to generate and then set the value of “myLIudf3”:

 

   Result = Me.PathForJobFiles

   If Result <> "" Then

           CType(RootPart.Properties("myLIudf3"), PropertySF).InputValue = Result

   End If

 

Whenever you need to reference a UDF property it must be always referenced via the RootPart object as shown above.

 

To restrict the values allowed to be chosen in a UDF to a list use the TableName and FieldName settings of the UDF. They allow you to map choices from the given TableName's FieldName into a drop-down selection list.

 

NOTE:

Use a view on the DB to create a "virtual" table with one column to use here if you don't have all the choices in one column of one table currently. Using a view will execute a SQL query to get the list.

 

Using a LineItem UDF value to pass a Value to Release.bat

 

Using the UDF from above, assume that there are two Project UDFs and three LineItem UDFs.

 

The UDF values are passed to the Release.bat file’s command line.  Since a third LI UDF is more than the %1 thru %9 command line arguments Rulestream can reference, use the shift command in the .bat file:

 

REM **

REM       Release.bat

REM       This file is executed as a part transmitting a lineitem.

REM       The first 6 parameters to this file are 'Release' path,

REM       Project ID, LineItemID, and Release ID, Release Type ID,

REM       and UserID that did the Release, respectively.

REM       The next 4 are UDF 1 thru 4 if they exist,

REM       starting with Project UDFs, then LIUDFs

REM

REM       Below is a sample of how the arguments might be used to execute different commands.

REM       This file is expected to be located in the Master Docs folder.

REM **

@Echo On

Echo Arguments passed in:

 

Echo %1 is the release directory

Echo %2 is the Project ID

Echo %3 is the lineitem ID

Echo %4 is the release ID

Echo %5 is the Release Type ID (from Release_Type table in ProjectDB)

Echo %6 is the UserID that did the Release

Echo %7 is the 1st UDF, starting with ProjectUDFs

Echo %8 is the 2nd UDF

Echo %9 is the 3rd UDF

 

REM To access arguments higher than (percent)9, you have to use the shift command

REM to shift the arguments one at a time to lower numbers.

REM For example, to get to the 10th argument, you would add the following:

REM

REM shift /8

REM (percent)9 now contains the 10th argument

REM

REM details are here:

REM http://www.microsoft.com/resources/documentation/windows/xp/all/proddocs/en-us/percent.mspx?mfr=true

 

shift /8

Echo %9 is the 4th UDF

 

shift /8

Echo %9 is the 5th UDF

REM Copy files from the Release folder to the folder specified in UDF5

Echo Preparing files for transfer from %1 to %9...

copy /Y "%1~\*" "%~9"

Echo File Transfer complete.

 

REM the ~ between the percent sign and the argument number removes any embedded double quote characters

 

REM @Echo On

REM Echo Executing the Released release.bat file...

 

REM "%~1GeneratedRelease.bat" %~1 %2 %3 %4 %7 %8 %9

 

Exit

Contributors