cancel
Showing results for 
Search instead for 
Did you mean: 

Femap Tips & Tricks: Coincident Node Move Only Option

Community Manager Community Manager
Community Manager

Sometimes you may need to set up a model to have a set of coincident nodes which can be connected together using spring or gap elements. To help prepare such a model, Femap includes a method of moving nodes to be coincident within a tolerance. See how you can use Femap’s Move Only, No Merge option of the Check Coincident Node capability to achieve this.

Femap Coincident Node Move Only Option

Alastair

Follow Femap on facebook and the Femap group on LInkedin