Cancel
Showing results for 
Search instead for 
Did you mean: 

NASCAR Analysis, RP & PLM at Hendrick Motorsports

Community Manager Community Manager
Community Manager

Jim Wall, director of engine engineering at Hendrick Motorsports, presented at PLM Connection on analysis and PLM in NASCAR.

I caught up with him after his presentation for this video clip.



Jim noted that one of the biggest design challenges they face is “keeping up with the pace of change” to be a winning team.

One of the more interesting parts of his presentation was the use of stereolithography rapid prototyping. They produce a full scale resin V8 engine that can fire.

He noted that there is so much data created in their business that a big challenge is to manage that data along with the “technical memory” of their team. They leverage a wireless Teamcenter web client that allows them to record an issue right on the track that instantly creates a workflow so they can begin improvements as soon as possible.

Some compelling stats:


Comments
Not applicable

great post.

Not applicable

I’m a fan of Formula 1 rather than NASCAR but the challenges are the same in keeping up with the latest technological advances in the science of racing. Stereolithography has been a growing part of F1 for about 2 years now, and it definitely showed this past season with a more open field of competition.