Cancel
Showing results for 
Search instead for 
Did you mean: 

NX Synchronous CAE – Part 3 - CFD

Siemens Legend Siemens Legend
Siemens Legend

This is part 3 in the series “NX Synchronous CAE”.  In this post, I would like to discuss how Synchronous Technology can be useful in CFD (computational fluid dynamics)

Analysts face a unique situation with CFD.  Designers only provide geometry of the part itself. The geometry needed for CFD analysis needs to be generated in an extra step.  CFD analysts need geometry representing the fluid domain - typically the voids within a part.

Traditionally, analysts go through many time consuming steps to create the fluid domain geometry, such as defining a bounding volume, executing a Boolean operation to subtract the original geometry, and then cleaning up the geometry.  This process along with the limited geometry capabilities of most CAE tools have presented challenges to CFD analysts.

Further, in traditional systems, whenever the original part design changes the analyst has to go through all these time consuming steps to update the CFD model.

NX CAE and NX Design Freedom powered by Synchronous Technology greatly simplify the process.



I’d like to thank my colleagues Ravi Shankar and Jeff Leidlein for providing the background information and video’s for this multi-part series on Synchronous CAE.

Comments
Not applicable

I worked with nx several years ago. I didn’t know there is cfd in it now. seems to be very interesting!

regards…

Siemens Legend

We have had CFD since NX 4.  It is based on the proven capabilities of I-deas CFD. (+10 years)