Cancel
Showing results for 
Search instead for 
Did you mean: 

Space system dynamic analysis presentation at the 2013 Femap Symposium

Community Manager Community Manager
Community Manager

MAYA Heat Transfer Technologies Limited and Preissner Engineering and Consulting LLC are teaming up to present at the Femap Symposium on 27th June. Eric Preissner of PEC will be discussing how Femap was used in a study of the dynamic response of the Landsat 8 satellite ground transport/handling system – a large system analysis in a dynamic design process with many iterations.

If you haven’t already registered for the Femap Symposium, do so now - there's just over a month to go. This presentation also illustrates how the Femap with NX Nastran Structural Analysis Toolkit helped with this study, and demonstrates how you can use the Femap API with an Excel application to drive model modifications.

Femap FEA model of the Hessi spacecraft
Primary Structure of the Hessi Spacecraft




The Femap Symposium is being held at the Cincinnati Marriott at RiverCenter, Covington, Kentucky on June 26 and 27th. Register now to secure your place at this great event and find out more about using Femap with NX Nastran, the Structural Analysis Toolkit and the Femap API in a dynamic response analysis.

Alastair