Cancel
Showing results for 
Search instead for 
Did you mean: 

Three Quick Reasons To Visit Local Motors At The SEMA Show

Genius
Genius

Local Motors is in row 37000 of the SEMA Show.  Its easy to find. just go south!  South hall. South side.  Here is why you want to visit:


  1. Cool cars - two are Rally Fighters, two are community built vehicles. One is Tandem.

  2. Community – Don’t just talk to Local Motors, talk to the people involved in building and designing their own vehicles.

  3. Free Trial of 3D CAD software – Local Motors partners like Siemens PLM have worked together to help put real design tools into the hands of people that like to design and build real stuff. Local Motors can show you how in a way that doesn't break the bank.


If you can’t make it to the SEMA show,  at least go check out their web site at http://Localmotors.com .  There are lot of pics and community projects already underway.

And if you need real CAD software, visit http://localmotors.com/D1 and download the free trial of Solid Edge Design1.  See how easy design can be with Siemens PLM’s new Synchronous Technology.