Cancel
Showing results for 
Search instead for 
Did you mean: 

André and Armand would have liked LMS Imagine.Lab

Siemens Visionary Siemens Visionary
Siemens Visionary

Figure1_PSA_Case_Study.pngA lot has changed since André Citroën and Armand Peugeot started making cars in 1919 and 1889 respectively. The car was still a concept when Armand Peugeot made four (!!!!) three-wheeled, steam-powered cars in 1889. Nice idea, but the trike-car was not a huge success. Steam wasn’t the right direction and the next Peugeots were four-wheeled cars with a petrol-fuelled internal combustion engines. Most notably, these Peugeots built in the 1890s were much more sophisticated with rubber tires, three-point suspensions and sliding-gear transmissions.

 

Both guys seem to have been turn-of-the-century petrol heads. While Armand Peugeot leaned towards racing -- a 3-horsepower Peugeot even won the world’s first motor race, the Paris-Rouen Competition for Horseless Carriages sponsored by Le Petit Journal in 1894, André Citroën followed the footsteps of Henry Ford. He introduced the first mass vehicle production line outside the United States. Not only were the early Citroëns numerous and priced to sell, André Citroën liked the marketing side of things, opening a showroom on the Champs-Élysées in Paris, using the Eiffel Tower for giant-sized advertising, and creating a sales and support concept similar to what we call dealerships today.

 

PSA_Engine.pngA hundred years later, this is all pretty crazy to think about. Modern cars are rolling computers with software running practically every system from the engine to the safety features to the climate control. And all these systems are becoming increasingly complex, and include a growing number of actuators, sensors, hybrid traction systems, and electric and electronic components, requiring controls and protection strategies to limit component damage without forgetting fuel efficiency and low emissions. How to engineer all this is an entirely different issue than what André and Armand had to deal with a century ago.

 

Luckily PSA Peugeot Citroën started using LMS Imagine.Lab Amesim software in 1995, the mechatronic system simulation platform from Siemens PLM Software.

 

Read more about how  PSA Peugeot Citröen enhances fuel efficiency of powertrain components