Cancel
Showing results for 
Search instead for 
Did you mean: 

Reach 50% efficiency of your off-road engines with system simulation

Community Manager Community Manager
Community Manager

Fit with total cost of ownership objectives complying with emissions regulations

Even if we are currently hearing a lot about electrification, off-road machines remain mainly powered by the internal combustion engine (almost nearly 100% for construction equipment). However, pollutant emissions from combustion engines significantly contribute to air pollution by emitting carbon oxide (CO), hydrocarbons (HC), nitrogen oxides (NOx), and particulate matter.

 

In 2019, a new European regulation enters into force: Non-Road Mobile Machinery (NRMM) makers have no choice but to introduce machine with engines complying to strict criteria that Stage V implied (Fig1). Industrial actors had several years to get prepared to progressively reduce the pollutant emissions and to phase out equipment with the most polluting engines.NRMM_worldwide emissions standards.pngSource: Delphi Technologies – worldwide emissions standards. On and off-highway commercial vehicles – 2018/2019

In parallel, OEMs still need to comply with the total cost of ownership reduction objectives, meaning improving fuel efficiency. By 2020, they may reach the 50% engine efficiency target – positioned between 30-40% today. This requires investigating several means for OEMs and engine suppliers.

 

Technical requirements are complex to find out the right balance between emission regulation compliance and fuel efficiency target. Combined with a competitive environment, off-road machines makers have to rethink their engineering process to be able to analyze their engine design early in the development cycle.

 

Opting for system simulation and focus on specific areas

So, in the context of fuel efficiency optimization, while complying with emissions regulations, there are several areas where the use of system simulation can accelerate product innovation such as:

  • In-cylinder
  • Thermal Management
  • After-treatment
  • Electrification
  • Intake, Exhaust & engine actuation
  • Powertrain integration

In the on-demand webinar Reach 50% efficiency of your off-road engines while complying with emission regulations Romain Nicolas from Siemens PLM Software and Bakir Puran from Liebherr Machines Bulle cover two of the identified areas above.

  • Firstly, Bakir Puran covers the waste heat recovery system design and analysis and how system simulation is used to simulate the organic Rankine cycle system. Indeed, it is known that an internal combustion engine produces a lot of heat which is not converted into mechanical or electrical power. In that case, the waste heat recovery system can turn one part of those heat losses into useful energy. This technology is an efficient way to reduce fuel consumption and so to reduce CO2 emissions. Liebherr Machines Bulle investigates that system optimization using Simcenter Amesim. Discover how and the results they achieved!
  • Secondly, focusing on after-treatment system design is fundamental to meet performance and reliability target, while optimizing fuel economy and cost savings. The use of simulation is a key asset to develop efficient engines and associated after-treatment design system in shorter delays. In that part, Romain does a live demonstration of how to optimize an after-treatment system and its thermal management using Simcenter Amesim.

Simcenter_Amesim_for_Large_Engine_HE_Optimization.pngSimcenter Amesim for Off-road large engine optimization

You wish to have a look at another area where you can optimize your fuel efficiency. Register to our other on-demand webinar: System simulation: a key differentiator for designing electrified heavy equipment