Cancel
Showing results for 
Search instead for 
Did you mean: 

Simcenter STAR-CCM+ v13.02: What's New?

Community Manager Community Manager
Community Manager

The latest release of Simcenter STAR-CCM+ is focused on helping you to engineer innovation.

 Template-banner-900x600.jpg

 

 

With v13.02, you will have stronger insight into key influences on your product’s performance through interactive and immersive exploration of simulation results with a new Virtual Reality Client. This release also brings significant gains in productivity with simulation workflow enhancements and reductions in overall time-to-solution, enabling you to conduct design exploration studies with ease and deliver innovative products that exceed customer expectations.

 

Simcenter STAR-CCM+ v13.02 benefits and features at a glance:

 

 

Make better design decisions with Immersive Virtual Reality

Your ability to make meaningful design decisions often depends on how quickly and easily you can interpret simulation results, and communicate that information to other stakeholders, many of whom do not regularly interact with simulation software.

 

Simcenter STAR-CCM+ v13.02 changes this forever by introducing a new immersive Virtual Reality environment through which anyone - independent of software experience - can explore and experience simulation models and data in a way that is simply not possible with mouse and keyboard manipulations.

 

Working with commodity VR hardware, you can now use hand gestures and head movements to become completely immersed in your model and explore it in a natural way. This immersive experience not only gives a much deeper understanding of your simulation results, it also allows you to rapidly troubleshoot problems on the spot.

 

For example, you can:

  • review your geometry and mesh quality by "walking through" your model
  • easily locate recirculation zones that adversely affect product performance by injecting massless particles that follow the flow paths within your model
  • identify human risk factors such as harmful exhaust fumes or smoke by placing yourself directly inside the environment

Ultimately, the insight gained from exploring your model in this way helps you make better design decisions faster and with more certainty than ever before.

 

 

Return to top. ^

 

Drive innovation with design exploration

To extract maximum value from your simulation, you need to be performing extensive design explorations studies that predict how your product will perform over all possible design configurations.

 

This process becomes even easier (and more robust) in the latest release, with the introduction of CAD robustness studies in Design Manager, which allow you to quickly identify potential errors in parametric models before conducting a design exploration study. CAD robustness studies ensure that the CAD model is tolerant to the full range of possible design changes, avoiding lost time and resources from failed CAD and giving confidence in finding better designs.

 

 

Simcenter STAR-CCM+ v13.02 also introduces new analysis capabilities which allow you to better understand design dependencies and quickly identify common design trends. During a design exploration study with Design Manager, you now have access to parallel plots linking design and response variables for each variant. You can overlay lines to compare multiple designs and synchronize them with plots for a deep dive into the results.

 

Return to top. ^

Increase productivity and reduce time-to-solution 

Your simulations can only drive innovation in the product development process if you deliver results on-time, every-time. Simcenter STAR-CCM+ v13.02 significantly increases your productivity through simulation workflow enhancements that deliver faster simulation throughput.

 

This release delivers a brand-new search tool to help with dissecting complex assemblies, saving significant engineering time. You can now find and filter faces in any model based on geometric, diagnostic or simulation data, and use this filter to repair a surface or extract information to use in the rest of the simulation.

 

Simcenter STAR-CCM+ v13.02 also reduces overset simulation time by up to 5x when modeling applications with objects in close proximity such as throttles and valves. In these cases, near wall cells automatically shrink to achieve an optimal size in the overset gap, allowing overall fewer cells while still maintaining physical accuracy.

 

Return to top. ^

 

Enable enterprise collaboration with PLMXML import

People, models, and data need to be connected to efficiently tackle the innovation of complex products. To this end, Simcenter STAR-CCM+ v13.02 has significant enhancements for PLMXML import, now supporting all types of PLMXML schemas. This facilitates robust connectivity to Teamcenter, Siemens’ widely used PLM software. With v13.02, you can now easily retrieve models and data, run an analysis and store the results back into Teamcenter. This enables full simulation and data management as part of the wider organization, facilitates dissemination of best practices among various teams regardless of location, and gives a more holistic view of the product across your organization. 

 

Return to top. ^

 

For information on all of the new features or to download Simcenter STAR-CCM+ v13.02, please visit the Steve Portal.

Comments
Experimenter
Hi Stephen, I have trouble in locating the download of trial version of Star CCM+. I am being directed to https://mdx.plm.automation.siemens.com/star-ccm-plus which doesn't work. Also the Steve Portal links provided in this community doesn't work either. Could you please help me out...? Thank you! Rohini.
Solution Partner Experimenter

@aarkay, You  need to sign up to the GTAC with your webkey and password If you arleady are a customer to download STAR-CCM+.

https://download.industrysoftware.automation.siemens.com/