Cancel
Showing results for 
Search instead for 
Did you mean: 

Spacecraft acoustic testing: Getting the spacecraft safe and sound into space

Siemens Theorist Siemens Theorist
Siemens Theorist

Simcenter Environmental Testing Satellite Launch.jpgSimcenter Environmental Testing Satellite Launch

 

A blog post on acoustic testing of satellites might be more interesting if I give you some background first. If you are thinking to build a spacecraft (whether it is to create a new telephone company, spy on your neighbor or help the world to improve weather forecast), you need to think also on how to get the spaceship up there! Nowadays, there is no shortage of choices for a launch vehicle: micro, mini, small or full-size satellites (or payload as they call them) have several carriers to reach space. From the media-champion Space-X company (with its Falcon 9), to Ariane work-horse, to the iconic Delta or the smaller Vega, you can find the launcher that fit your budget (and weight!)

 

Spacecraft launch.jpg

 

Once you sign with a launcher company, you’ll get a pack of documents, one of which is the launcher user manual. As any user manuals, this document tells you what to do with your product. For example, chapter 4 of the Ariane 5 User’s manual details: “The design and dimension data that shall be taken into account by any customer intending to launch a spacecraft compatible with the Ariane 5 launch vehicle”. A few pages later you will find this: “The spacecraft authority shall demonstrate that the spacecraft structure and equipment are capable of withstanding the maximum expected launch vehicle ground and flight environments. The spacecraft compatibility must be proven by means of adequate tests.”

 

Spacecraft verification and qualification test campaign.jpgSpacecraft verification and qualification test campaign; source: Ariane 5 User’s Manual

 STM = Structural Thermal Model ; FM = Flight Model; PFM = Proto Flight Model

 

In other words, if you want to launch a satellite, you have to test it! And that’s where Siemens comes into the picture. Yes, our dynamic environmental testing solutions, is used to test satellites. Did you know that the majority of satellites produced in Europe, Japan, China, India, Russia, US are tested with Siemens Simcenter SCADAS hardware in conjunction with Testlab software?

 

The essentials of vibration and acoustic testing of spacecrafts

 

Now, one of the tests to be done, as indicated by the table above, is acoustics. The noise level generated at launch is not only lethal to humans, but it can also damage the payload...or in another words, the whole space mission can be compromised. And nobody wants that! The Overall Sound Pressure Level (OASPL) reaches 146dB inside the fairing (where the spacecraft is tucked up to go to space). This vibration value can cause structural damages and jeopardize the functionality of instruments and subsystems. To give you an idea, 146dB is about 20 times louder than an operating jackhammer…with no ear protection! So, before the spacecraft launch, the large and flexible components of the launch vehicle (for example reflectors, or solar panels) as well as the Proto-Flight (PF) model, are tested and exposed to high intensity noise. In this way engineers can assess their response and ensure they will survive the launch.

Spacecraft launch noise levels Simcenter.jpgSpacecraft launch noise levels reach 146 dB

On one hand these ‘payload vibro-acoustic tests’, as defined in the NASA Handbook, have been historically carried out in unique reverberant acoustic test facilities. While on the other hand, during the last decade there is a growing interest, with some technological leap, to develop alternative satellite test equipment and methods. Let me tell you a little bit about the known-accepted-standard way and something about the newer testing method.

 

Reverberant Field Acoustic Excitation (RFAX): The established satellite testing process

ESA Reverberant Field Acoustic Excitation (RFAX).jpegEuropean Space Agency (ESA) Reverberant Field Acoustic Excitation (RFAX) testing method

The conventional method of ‘payload vibro-acoustic tests’, sometime referred to as RFAT - Reverberant Field Acoustic Test, requires large reverberant acoustic chambers. (See the photo above showing the room at Thales Alenia Space in Cannes.) As the satellites have been launched for decades using this type of tests, this methodology is validated, accepted and part of the industry standards or handbooks.

Applying this spacecraft vibration testing method, Simcenter Testlab Acoustic Control makes sure that the noise generated in the chamber matches the profile imposed by the launcher user’s manual. The noise is generated by a set of acoustic modulators and ‘horns’, which together produce high-intensity pressure waves. These chambers have usually more than one modulator/horn. (NASA Plumbrook which is the biggest in the world, has 36 of them!!). Most of the rooms use nitrogen-filled room, whilst some used dried oxygen. The final goal is to keep the air as ‘clean’ as possible and minimize sound absorption.


As effective as RFAN tests can be, the sheer size of the building (fitting reverberant chambers of 1000cubic meter with 1m thick walls), the complexity of the gas/depuration system, the overall running cost and their geographical spread, make this choice to the spacecraft owner very onerous.

 

Direct Field Acoustic Noise (DFAN): A different spacecraft acoustic testing

Simcenter Direct Field Acoustic Noise (DFAN) Test Setup.jpgSimcenter Direct Field Acoustic Noise (DFAN) testing setup

 

For a purely business reason, companies in US started to ask the question: “What if we use loudspeakers to make that much noise?” That question was asked almost two decades ago. It took numerous series of tests and a many of broken speakers to reach today’s state-of-the-art satellite vibration test method. Based on Multi-Input-Multi-Output (MIMO) narrow-band control algorithms, SimecenterTestlab offers today the possibility to generate the required noise level (146dB) and field uniformity for spacecraft acoustic testing.  Of course, once that an adequate set of speakers and amplifiers is provided. The photo below shows a typical setup of tests with 96 loudspeakers and amps (check out the related case study here). Such a setup requires less cost compare to the investment and running cost of a reverberant chamber. What’s more, the main added value of the DFAN method is that the all sound system can be moved and transported to the manufacturing site. This is a great benefit since the payload doesn’t have to be shipped to the test facility. So, the economic benefit for spacecraft manufacturer is clear: no need to build very expensive test facilities, no need of moving payload and teams of engineers to a remote test center and increasingly efficient testing technology… However, the space agencies and launch vehicles producers are still trying to create the necessary guidelines for the industry. As of today, NASA Handbook 7010 is the only document that provide some guidelines.

 

Direct Field Acoustic Noise (DFAN) innovative spacecraft acoustic testing method.jpgSimcenter Direct Field Acoustic Noise (DFAN) innovative spacecraft acoustic testing method

As this innovative direct field acoustic excitation technology advances also in the control algorithms included in the Simcenter Testlab software, this attracted the main attention of satellite OEMs and agencies through a number of research activities, validation tests and scientific publications. The European Space Agency (ESA) is now fully aware of the full potential of this method. Surely there will be more to come.

 

Simcenter Testlab solutions for dynamic environmental testing.jpgComplete Simcenter Testlab solutions for dynamic environmental testing

 

To conclude, when building your next (or first) satellite, you will have to verify and qualify it also to acoustic excitation. Whether you opt for a standard reverberant chamber test facility or you proceed with more versatile and innovative technique, being a reliable partner in many projects applying both methods, you can count on our expertise. Learn more about dynamic environmental testing here.