Reply

Announcing Solid Edge 2D Drafting ST3

The latest version of Solid Edge 2D Drafting is available for download at
the free2D web site.
This is Solid Edge 2D Drafting ST3.
http://www.plm.automation.siemens.com/en_us/products/velocity/solidedge/free2d/index.shtml
A number of enhancements have been made.
The user interface is customizable.
You can move the command buttons in the command ribbon to make the UI more
logical for you.
Check out the new Radial Menu.
This is an on-screen menu that you can customize to put the commands you
want close to the cursor.
Just Right Mouse Click and hold. Then drag the mouse with the right mouse
button down.
The radial meny pops up at the cursor location. Drag around the menu to find
the command you want.
Let up on the mouse to execute the command. Try it with zoom area and fit.
It is currently configured for Solid Edge, so some of the commands wil be
disabled.
Have fun.
Rick B.

1 REPLY

Re: Announcing Solid Edge 2D Drafting ST3

Thank you for finally fixing the problem with the "Enable dimension changes using the mouse wheel." option. Disabling it in the past did not disable it. Now it works as it should. No more changing dimensions when I think I should be zooming.