Auto Save annoying feature

Valued Contributor
Valued Contributor

Hi Guys

One thing I find annoying with auto save is that the timer doesn't reset if I do a manual save.

And the prompt to autosave always seems to pop up in the middle of an action.

 Could the auto save prompt be programmed to delay until there is a pause in drawing and reset after a manual save?

 

Cheers

Pete

1 REPLY

Re: Auto Save annoying feature

Esteemed Contributor
Esteemed Contributor

AutoSave should already wait for a command to be complete before prompting.

 

I imagine that they could reset the timer based on a manual save but a request to do that would need to be turned in through the proper channel by a customer under maintenance.



Ken

Production: ST10 MP3
Testing: SE 2019