Batch Convert .dft to .dwg

N/A

I have several (actually, it's more like a couple hundred) files that I created using
Solid Edge. I now want to send these to someone who uses AutoCAD. I know I can
convert the files one by one, but is there a way to do a batch convert? Even a
script that would open the program, load the file, and do a save as..., or command
line options?
Thanks,
Chris
1 REPLY

Re: Batch Convert .dft to .dwg

N/A
If you are using the free version, no. The free version has the Application
Programming Interface (API) disabled so no macro or script will work. The
purchased version or full Solid Edge comes with a macro that will do what
you are asking.
--
PellaKen
http://grundey.blogspot.com
"Chris" wrote in message
news:477bcc32$1@bbsnotes.ugs.com...
>
> I have several (actually, it's more like a couple hundred) files that I
> created using
> Solid Edge. I now want to send these to someone who uses AutoCAD. I know
> I can
> convert the files one by one, but is there a way to do a batch convert?
> Even a
> script that would open the program, load the file, and do a save as..., or
> command
> line options?
>
> Thanks,
> Chris