Bill of materials using Table

N/A

Is there a procedure for linking a dimension from the drawing or variable table to
a cell in the Table feature? I am making up a bill of materials, and it would be
a natural feature to allow such linking, which would update the bill of materials
if a dimension is modified. If not, host please consider this as a feature request!
John Hilgenberg
1 REPLY

Re: Bill of materials using Table

N/A

I see some instructions about linking to a spreadsheet. I'll try that and come back
if I have any trouble.
"John Hilgenberg" wrote:
>
>Is there a procedure for linking a dimension from the drawing or variable
>table to
>a cell in the Table feature? I am making up a bill of materials, and it would
>be
>a natural feature to allow such linking, which would update the bill of materials
>if a dimension is modified. If not, host please consider this as a feature
>request!
>
>John Hilgenberg

John Hilgenberg