Can ST3 run on Windows 7 64 bit?

N/A
Hi,
I keep getting a message that the program cannot find a valid licence yet I have put it into program files(x86)/solid edge xxxx/program
This is where the licence file resides on a 64 bit system.
Anybody know if this is possible to run on 64 bit?
Thanks,
Andrew
3 REPLIES

Re: Can ST3 run on Windows 7 64 bit?

N/A
Andrew,
Are you trying to run ST2 or ST3?
What operating system are you trying to run on?
Is this a new installation of 2D Drafting, or have you been running for a
while?
Regards,
Rick B.

Re: Can ST3 run on Windows 7 64 bit?

N/A
ST3 which is the most recent release seems to work just fine on my Win7 Pro 64bit laptop, this was installed before I downloaded and installed the XP mode so I know it was running on Win7. It did install into the Program files (x86) folder which means it is probably a 32bit application, but it does run. I haven't done much more than draw a few doodles to see if it was working, haven't taken the time to move old drawing over and check to make sure they still function (but I don't think there will be a problem).
The only thing I had to do was to temporarily disable UAC and reboot, just punch UAC into the windows search box and it will lead you to the process.

Re: Can ST3 run on Windows 7 64 bit?

N/A
Solid Edge 2D Drafting is a 32bit application.
But it does run on a 64bit machine.
You should not have any problems.
We deliver Solid Edge in either 32bit or 64bit.
We only deliver 2D Drafting in 32bit.
Regards,
Rick B.