Reply

Can't Measure Geometry


When I open a .dft file created in V19 Solid Edge, I can't measure the geometry with
the 2D Draft package. It won't allow me to select any geometry. Is this the way
the software is suppose to function or is there a fix?
1 REPLY

Re: Can't Measure Geometry

Ken,
This is by design. You can open any Draft file created with Solid Edge in
Solid Edge 2D Drafting. Everything displays as it does in Solid Edge. But
the drawing views are disabled. Solid Edge 2D Drafting is not intended to be
used as a drafting tool for drawings created from 3D Solid Edge models. It
can be used as a collaboration tool. With this in mind, drawing views are
protected information. A draft file could be sent to a supplier or someone
else in the organization. The supplier can open the draft file with a free
copy of Solid Edge 2D Drafting. The supplier can add comments and mark the
file up. He can save the file and send it back to the person it came from.
The supplier can also plot the original drawings. The original sender can
open the modified file and review the markups. The beauty of this is that it
is all the same file. There is no need of translating the file to another
format. There is always a possability of loss of data during translation.
Rick B.