Reply

Can't run free 2D ST3.

When I launch Free 2D ST3, I get the following message:

Solid Edge 2D Drafting could not find a valid license ...

Using this license file with ST2 works fine.

When I open the license file, the first line is:
INCREMENT solidedge2ddrafting sedemon 102.0 01-apr-2011 uncounted \

May this be the problem ? The license file seems to be only valid with ST2 ?

Regards,


Michel
4 REPLIES

Re: Can't run free 2D ST3.

When you install you should not have to do anything with the license.
Installation does it for you.
The license installed by setup is the V103 license.
Simply install and run the software.
Regards,
Rick B.

Re: Can't run free 2D ST3.

Hi Rick,

You're right. The license provided with the install is V103 and works fine.

The problem I see is if people click on the link to update their license, they will get the one for V102.
I think it will make sense to update this link to get a V103 license.

Anyway, problem solved.

Regards,


Michel

Re: Can't run free 2D ST3.

I am working on getting the download license updated.
It should be updated to the V103 license within a couple of days.
Regards,
Rick B.

Re: Can't run free 2D ST3.

I did things oppositely... I downloaded both the license and the complete package thinking that if the package didn't provide a license (ie it failed) I would then try the license file. Never needed the license file since the ST3 install provides a new one and the computer was brand new (never had any version of SE 2D on it.)