Cannot install SE Free

N/A
I've downloaded Solid Edge Free 2D but when I attempt to install, I get this messagebox:

---------------------------
InstallShield DLL Custom Action
---------------------------
File 'C:\DOCUME~1\rhaggard\LOCALS~1\Temp\_is4A.tmp' can not be found. Make sure the file is on target system or installed already.
---------------------------
OK
---------------------------

Looking at that directory, I do not see __is4A.tmp. Any ideas why installation fails?
1 REPLY

Re: Cannot install SE Free

N/A
Before running the SE installation, .NET 3.5 must be installed. This can be downloaded from here:

http://www.microsoft.com/downloads/details.aspx?FamilyId=333325fd-ae52-4e35-b531-508d977d32a6&displa...

If this link is not valid then simply search Google for ".NET 3.5 install" and you should find a download link very near the top.