Cannot place dimensions on draft

Creator
Creator

Hey,

We received a .dft file which was done with ST9. We can open it and we actually can change the dimensions which are already placed but we cannot place new ones. We cannot do anything with the principal views (select, delete, place dimension etc.). Anyone has any guesses why?

 

We also got the .psm model file but there was no link in the .dft to update. My guess was that the views have been converted to 2D but we still should be able to place dimensions from there or at least delete the whole view.

3 REPLIES

Re: Cannot place dimensions on draft

Community Manager Community Manager
Community Manager

Make sure your license is correct. It sounds like you are using a Free 2D Drafting license. 2D Drafting will dumb down the software. An easy way to tell is to see if you have all of the drawing view placement commands.

 

Rick B.

Re: Cannot place dimensions on draft

Esteemed Contributor
Esteemed Contributor

If running the Free 2D Drafting license of Solid Edge, I believe one of the restrictions is that you cannot annotatate/dimension views placed from a 3D model as it only allows for viewing those type of drawings.  Free 2D Drafting is meant to be used for a 2D only workflow not involving 3D models.



Ken

Production: ST10 MP3
Testing: SE 2019

Re: Cannot place dimensions on draft

Creator
Creator

Wow, thanks guys!

We actually have a limited number on licenses in our company and when all are in use we use the 2D license, which is free.