Reply

Changing a Distance Between dim: which moves?

I've dimensioned the distance between two parallel lines. One line is (I think) unconstrained by other relationships and one is connected to other geometry. When I change the value of the dimension, the connected line moves, no matter how I attempt to tie down that line with relationships, constraints, etc. I tried playing with this with a couple of free lines elsewhere and I had no control over which line would move. Is there a way to specify which element is to move when a driving dimension is changed?
2 REPLIES

Re: Changing a Distance Between dim: which moves?

You can place lock constraints to lock down the position of keypoints on
objects.
In the Relate command group it looks loke a pad lock.
Regards,
Rick B.

Re: Changing a Distance Between dim: which moves?

Works like a charm. Thanks, Rick!