Circular Pattern Tool Bug?

N/A

Is there a known bug with the circular pattern tool? See attached bad image. the
only way I could get the circular pattern tool to place that pattern correctly was
to delete the horizontal/vertical constraints from the lines that make up the notch.
I don't remember having this problem with the previous version of Solid Edge 2D.
Thanks,
Ed

3 REPLIES

Re: Circular Pattern Tool Bug?

N/A

And here is the good image. (the bulletin board doesn't seem to allow attaching more
than one image to a post.)
Ed
"Ed Kadlec" wrote:
>
>
>
>Is there a known bug with the circular pattern tool? See attached bad image.
>the
>only way I could get the circular pattern tool to place that pattern correctly
>was
>to delete the horizontal/vertical constraints from the lines that make up
>the notch.
>I don't remember having this problem with the previous version of Solid Edge
>2D.
>
>Thanks,
>Ed


Re: Circular Pattern Tool Bug?

Siemens Pioneer Siemens Pioneer
Siemens Pioneer
Ed,

I am able to reproduce a problem even in the fully licensed version of Solid Edge Draft and will log a problem report to development for it. I was not able to view your image (it tells me I do not have permissions, for what I do not know). Anyway, I created a circle and drew a "notch" at the top consisting of two vertical and one horizontal lines. I then patterned this with a count of 6 occurrences and the one at the bottom is not oriented correctly. If I delete the horizontal and vertical constraints on the original lines, then I get the correct answer.

Like I said, I will have development take a look at this.

Andy.

Re: Circular Pattern Tool Bug?

N/A

Andy,
If you go to the old bulletin board you can view the images. But, you were able
to reproduce the problem so it's probably not necessary.
Maybe you could also log a problem report for the bulletin board image issue.
Thanks,
Ed
andrew.brezinski@siemens.com
wrote:
>
>Ed,
>
>I am able to reproduce a problem even in the fully licensed version of
>Solid Edge Draft and will log a problem report to development for it. I
>was not able to view your image (it tells me I do not have permissions,
>for what I do not know). Anyway, I created a circle and drew a "notch"
>at the top consisting of two vertical and one horizontal lines. I then
>patterned this with a count of 6 occurrences and the one at the bottom
>is not oriented correctly. If I delete the horizontal and vertical
>constraints on the original lines, then I get the correct answer.
>
>Like I said, I will have development take a look at this.
>
>Andy.