Creating a ring with notches out of it...

N/A
Hi - I'm just starting with SE 2D, and am a bit stuck with creating a ring (two concentric circles, 125mm & 165mm) - I want 8 equidistant notches into the outside of the outer ring, 10mm x 3mm.

I'm having real problems. Help would be appreciated.

Windows 7, latest SE 2D

Many thanks

Nick
4 REPLIES

Re: Creating a ring with notches out of it...

N/A

Nick,
See attached image. If this is what you are trying to do then I would use the circular
array tool to create what you need.
Ed
nick@desmith.net wrote:
>
>Hi - I'm just starting with SE 2D, and am a bit stuck with creating a
>ring (two concentric circles, 125mm & 165mm) - I want 8 equidistant
>notches into the outside of the outer ring, 10mm x 3mm.
>
>I'm having real problems. Help would be appreciated.
>
>Windows 7, latest SE 2D
>
>Many thanks
>
>Nick


Re: Creating a ring with notches out of it...

N/A
For some reason I cannot open the attachment, even when logged in. It also seems I can't post attachments - annoying as There is a problem that I want to discuss and to upload an example image.
Cheers
Nick

Re: Creating a ring with notches out of it...

N/A

Nick,
I couldn’t view it using the new bulletin board either. The image displays automatically
in the old bulletin board. I normally use the old bulletin board. I emailed the
image to you.
Ed
nick@desmith.net wrote:
>
>For some reason I cannot open the attachment, even when logged in.
>
>Cheers
>
>Nick
>
>
>--
>nick@desmith.net
>------------------------------------------------------------------------
>nick@desmith.net's Profile: http://bbsnotes.ugs.com/vbulletin/member.php?userid=124553
>View this thread: http://bbsnotes.ugs.com/vbulletin/showthread.php?t=42331
>


Re: Creating a ring with notches out of it...

N/A

Oops! I mean "Circular Pattern" tool.
Ed
"Ed Kadlec" wrote:
>
>
>
>Nick,
>
>See attached image. If this is what you are trying to do then I would use
>the circular
>array tool to create what you need.
>
>Ed
>
>nick@desmith.net wrote:
>>
>>Hi - I'm just starting with SE 2D, and am a bit stuck with creating a
>>ring (two concentric circles, 125mm & 165mm) - I want 8 equidistant
>>notches into the outside of the outer ring, 10mm x 3mm.
>>
>>I'm having real problems. Help would be appreciated.
>>
>>Windows 7, latest SE 2D
>>
>>Many thanks
>>
>>Nick

>