DATA EXTRACTION FROM D3 PART MODEL

Experimenter
Experimenter

Hi,

I just wanted to know that the data which is fed into while creating holes on the 3D model can it be extracted completly,

Example: In the hole Command while selecting it ask for different types of options like ,Standard,Size,type of hole,etc.

suppose in which i feed the data in the following manner.

 

                                       Standard-ANSI Inch

                                       Size;-1/4"unc,etc

 

Now from above fed data i am interested in knowing whether the above details can be refelcted in the draft environment of that particular part or not.

1 REPLY

Re: DATA EXTRACTION FROM D3 PART MODEL

YES,

 

in the Draft, find the Call Out command,  within you will find Hole Callout  which will annotate the 3D Hole. 

===================================================
Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.6