Datum Dimensions

N/A

When using datum dimensioning, how do you keep the dimension lines and text from
overlappping when they are pointing to features that are adjacent? Can a jog be
put into the leader?
Paul Hundt
SiGn Innovations
1 REPLY

Re: Datum Dimensions

N/A
Paul,
By datumn dimension, I assume you are talking about placing dimensions with
the Coordinate Dimension command.
If so, you can add joggs to the dimensions after they are created.
Click on the dimension that you want to add the jog. The dimension will be
selected.
Put your cursor on the dimension projection line where you want to add the
jog.
Press and hold the 'Alt' key on the keyboard and click on the dimension.
This adds a jog.
Note that this is for Coordinate Dimensions.
Regards,
Rick B.