Reply

Decimal Places in Property Text


I've just been trying to limit the number of decimal place shown in a property text
call out.
It's given a brief explanation in the help file, but I can't get this working:
You can use property text to control the number of decimal places in numbers. For
example, to set a number to display 4 decimal places, use the following format:
%{PropertyName or CustomPropertyNumber/@4|ModelRef}

So I tried to control the number of decimal places in the variable as follows:
(Before)
LENGTH: %{arc_allowance}
(After)
LENGTH: %{arc_allowance/@1}
But this gives no difference to the text displayed.
Does anyone have any experiance in using this method of only displaying the required
decimal places (in this case I don't want any decimal places: integer values only).
-AS

www.continual-motion.com
2 REPLIES

Re: Decimal Places in Property Text

Andy,
There is a current limitation with formatting custom properties in property
text. Custom properties are currently passed to Draft and therefore to
property text as string values not as a real values. Therefore, formatting
will not work because they are strings.
Regards,
Rick B.

Re: Decimal Places in Property Text


I've bypassed that through FILE>FILEPROPERTIES>UNITS>ADVANCEDUNITS
And nominated clone variables as Scalars which I can then control number of decimal
places with.
(pull down menus, .12 etc)
I think this thread is closed down, but there is another one along similar lines
I'm about to post (Updates of Property Text)
-AS

"Ricky Black" wrote:
>Andy,
>There is a current limitation with formatting custom properties in property
>
>text. Custom properties are currently passed to Draft and therefore to
>property text as string values not as a real values. Therefore, formatting
>
>will not work because they are strings.
>
>Regards,
>Rick B.
>
>

www.continual-motion.com