Reply

Delete duplicate lines


When I paste, rotate or move an element multiple duplicate line are created.
Trimming or deleting these requires that the operation be repeated many times.
What am I doing to cause this?
Is there means in 2-d to select and remove multiple elements in a single operation?
Thank You,
John

1 REPLY

Re: Delete duplicate lines

Not sure what you are doing, but the commands work with whatever is selected
so if you select more than you intended and do not watch the prompts, you
may get a lot more than you bargained for. Also be aware that some of the
tools like rotate or move has a copy option which will do just that.
To delete multiple elements you can use the Filter on the select tool to
turn off the items (like constraints) that you do not want to delete, then
fence all the objects to select them, then use the shift key + left mouse
button to deselect the item you do not want to delete.
--
Ken
http://grundey.blogspot.com
"John Buscher" wrote in message
news:47e2b71a$1@bbsnotes.ugs.com...
>
> When I paste, rotate or move an element multiple duplicate line are
> created.
>
> Trimming or deleting these requires that the operation be repeated many
> times.
>
> What am I doing to cause this?
>
> Is there means in 2-d to select and remove multiple elements in a single
> operation?
>
> Thank You,
>
> John
>
>