Reply

Dimension Properties


Good Afternoon
Is there a way that I can reset the Tolerance Text Size.
The default is 0.5, I want it 1.
Regards
Hendrik
2 REPLIES

Re: Dimension Properties

Hendrik,
The tolerance text size is a property of the dimension style. If you change
the style, it will change for all dimensions.
Click on Format at the top of the application window. Then click on Style.
This will display the Style dialog.
Change the Style type to dimension.
Click on the dimension that you use in the list.
Click the Modify button.
Click on the Text tab in the Modify Dimension Style dialog.
Change the Tolerance Text size to 1. Click OK. All your dimensions with
tolerance text should change.
If you need to change individual dimensions you may change the same property
in the properties of each dimension. This will override the style on the
dimension. If you have changed the property on specific dimensions, this
puts an override on those dimensions. The change to the style will not
remove the override.
If you always want all tolerance text on all dimensions set this wayfor all
files you create, you need to create your own template draft file. Set this
in your template. If you need more information about creating a template,
let me know.
Regards,
Rick B.

Re: Dimension Properties


"Ricky Black" wrote:
>Hendrik,
>The tolerance text size is a property of the dimension style. If you change
>
>the style, it will change for all dimensions.
>
>Click on Format at the top of the application window. Then click on Style.
>
>This will display the Style dialog.
>Change the Style type to dimension.
>Click on the dimension that you use in the list.
>Click the Modify button.
>Click on the Text tab in the Modify Dimension Style dialog.
>Change the Tolerance Text size to 1. Click OK. All your dimensions with
>tolerance text should change.
>If you need to change individual dimensions you may change the same property
>
>in the properties of each dimension. This will override the style on the
>dimension. If you have changed the property on specific dimensions, this
>puts an override on those dimensions. The change to the style will not
>remove the override.
>If you always want all tolerance text on all dimensions set this wayfor all
>
>files you create, you need to create your own template draft file. Set this
>
>in your template. If you need more information about creating a template,
>
>let me know.
>
>Regards,
>Rick B.
>
>

Thanks Ricky
Regards
Hendrik