Reply

Dimensions

Good morning,
Is there a way to stop the software automatically showing an offset
dimension when using the offset tool? I have automatic dimensions turned
off but when using the offset tool the offset dimension appears
automatically.
Many thanks
Roger
2 REPLIES

Re: Dimensions

Roger,
I don't believe there is a way to suppress creating the dimension.
Rick B.

Re: Dimensions

Rick,
That's a pity because after using the offset command a number of times
followed by the trim tool you are left with numerous extraneous
'dimensions' which visually 'get in the way'. Not a big issue because they
can be cleaned up manually but it would be nice not to have to.
The new version is an improvement on the earlier, still very good, version.
Many thanks,
Roger
"Ricky Black" wrote in message
news:4bacb424@bbsnotes.ugs.com...
> Roger,
> I don't believe there is a way to suppress creating the dimension.
>
> Rick B.
>