Does free version support Save As DXF or DWG?

N/A

I am using the free version of Solid Edge 2D Drafting and can see only a "Save As
... Image" option. Do I need to get a paid version in order to Save As DXF or DWG?
Thanks,
Dan
2 REPLIES

Re: Does free version support Save As DXF or DWG?

N/A

Dan,
Click on the "Save As" and a dialog window will pop up that allows you to select
the file type to save as. See attached image.
Ed
"Dan Bogen" wrote:
>
>I am using the free version of Solid Edge 2D Drafting and can see only a "Save
>As
>.. Image" option. Do I need to get a paid version in order to Save As DXF
>or DWG?
>
>Thanks,
>
>Dan


Re: Does free version support Save As DXF or DWG?

N/A

Ed,
Many thanks. I see how it works now.
Dan
"Ed Kadlec" wrote:
>
>
>
>Dan,
>
>Click on the "Save As" and a dialog window will pop up that allows you to
>select
>the file type to save as. See attached image.
>
>Ed
>
>"Dan Bogen" wrote:
>>
>>I am using the free version of Solid Edge 2D Drafting and can see only a

>"Save
>>As
>>.. Image" option. Do I need to get a paid version in order to Save As DXF
>>or DWG?
>>
>>Thanks,
>>
>>Dan

>