Cancel
Showing results for 
Search instead for 
Did you mean: 

Error during installation of SE 2D drafting ST3 - win7

N/A
Hello,
I have downoladed installer. After setup is run, I can choose destination folder and default profile. After that I click "Install" and then receive and error message "The wizard was interrupted before...." - pls see an attachment.
System: Win 7 Home Premium.
Does anyone have an idea what could be the root cause of this error? How could I eliminate this?

Thanks in advance for any info.
8 REPLIES

Re: Error during installation of SE 2D drafting ST3 - win7

Siemens Pioneer Siemens Pioneer
Siemens Pioneer
Hi Tomasz,

Go into Control Panel and look for your User Account Control. I am not sure where it will be exactly on Windows 7 Home Edition, but look for things like "Security" or "Software & Security", then Action Center, then "choosing your UAC". Make sure the UAC is set all the way down to "Never notify" and see if this gives you better results.

Good Luck!

Andy

Re: Error during installation of SE 2D drafting ST3 - win7

N/A
Hi,
I have UAC switched off and run installer with administrator's privileges.
I tried also run installer in windows xp compatibility mode. Without any change. At this moment I don't have other idea what could be the problem.

Re: Error during installation of SE 2D drafting ST3 - win7

N/A
Make sure you have administrator privelages.
Also make sure the UAC (User Account Control) is turned all the way down.
Try installing again.
When you download the software, click on the button to Save the download,
not Run.
This way you can Run it at any time.
After the download completes, it will aks you if you want to Run it.
Regards,
Rick B.
"zukowski.tomasz@gmail.com"
wrote in message
news:zukowski.tomaszgmail.com.4s1qvb@noreply.bbsnotes.ugs.com...
>
> Hello,
> I have downoladed installer. After setup is run, I can choose
> destination folder and default profile. After that I click "Install" and
> then receive and error message "The wizard was interrupted before...."
> - pls see an attachment.
> System: Win 7 Home Premium.
> Does anyone have an idea what could be the root cause of this error? How
> could I eliminate this?
>
> Thanks in advance for any info.
>
>
> +-------------------------------------------------------------------+
> |Filename: error.jpg |
> |Download:
> http://bbsnotes.ugs.com/vbulletin/attachment.php?attachmentid=3711|
> +-------------------------------------------------------------------+
>
> --
> zukowski.tomasz@gmail.com
> ------------------------------------------------------------------------
> zukowski.tomasz@gmail.com's Profile:
> http://bbsnotes.ugs.com/vbulletin/member.php?userid=324370
> View this thread: http://bbsnotes.ugs.com/vbulletin/showthread.php?t=45228
>


Re: Error during installation of SE 2D drafting ST3 - win7

N/A
Ricky,
all the requirements You have listed are met.
I had searched the web and tried several solutions but without success. I do not have any idea at this moment.
I have made usage of psr.exe and prepared detailed description when exactly this problem occurs --> see the attachment.
There is description in polish (polish version of Windows) but pictures also shows everything.
Maybe I'll find somebody who could help with some "magic" solution.

And I would also ask in another way: is here anybody who installed succesfully solid Edge ST2 (free 2D) on the computer with Windows 7 Home Premium operating system?

Thank You.

Re: Error during installation of SE 2D drafting ST3 - win7

N/A
Did you have a previous version of 2D Drafting, or is this the first time
you are installing?
Rick B.
"zukowski.tomasz@gmail.com"

wrote in message
news:zukowski.tomaszgmail.com.4tycjn@noreply.bbs.industrysoftware.automation.siemens.com...
>
> Ricky,
> all the requirements You have listed are met.
> I had searched the web and tried several solutions but without success.
> I do not have any idea at this moment.
> I have made usage of psr.exe and prepared detailed description when
> exactly this problem occurs.
> There is description in polish (polish version of Windows) but pictures
> also shows everything.
> Maybe I'll find somebody who could help with some "magic" solution.
>
> And I would also ask in another way: is here anybody who installed
> succesfully solid Edge ST2 (free 2D) on the computer with Windows 7 Home
> Premium operating system?
>
> Thank You.
>
>
> --
> zukowski.tomasz@gmail.com
> ------------------------------------------------------------------------
> zukowski.tomasz@gmail.com's Profile:
> http://bbs.industrysoftware.automation.siemens.com/vbulletin/member.php?userid=324370
> View this thread:
> http://bbs.industrysoftware.automation.siemens.com/vbulletin/showthread.php?t=45228
>


Re: Error during installation of SE 2D drafting ST3 - win7

N/A
This is the first installation. System *Win7) is quite "fresh" and Solid Edge has never been installed before.

Re: Error during installation of SE 2D drafting ST3 - win7

N/A
At this point I do not have an answer for you.
Others are not having this problem.
What virus scanning software are you running?
Rick B.

"zukowski.tomasz@gmail.com"

wrote in message
news:zukowski.tomaszgmail.com.4u05cz@noreply.bbs.industrysoftware.automation.siemens.com...
>
> This is the first installation. System *Win7) is quite "fresh" and Solid
> Edge has never been installed before.
>
>
> --
> zukowski.tomasz@gmail.com
> ------------------------------------------------------------------------
> zukowski.tomasz@gmail.com's Profile:
> http://bbs.industrysoftware.automation.siemens.com/vbulletin/member.php?userid=324370
> View this thread:
> http://bbs.industrysoftware.automation.siemens.com/vbulletin/showthread.php?t=45228
>


Re: Error during installation of SE 2D drafting ST3 - win7

N/A

And I would also ask in another way: is here anybody who installed succesfully solid Edge ST2 (free 2D) on the computer with Windows 7 Home Premium operating system?


I'm running Solid Edge 2D on my laptop which is running Windows 7 Home Premium. I've had no problems running it.

Ed