Error message

N/A
Hello

When I try to open a drawing by clicking a xxx.dtf file I get a message

"Please wait while Windows configures Solid edge 2D"
After a while I get a message
"The feature you are trying to use is on a network resource that is unavailable
Click OK to try again, or enter an alternate path to a folder containing the installation package 'Solid Edge 2D Drafting ST4.msi in the box below."

I can not find a .msi file. The program is installed from a free downloaded
SE2DDraftV104ENGLISH.exe file

When I start Solid Edge I can open a xxx.dtf file without problems. When I save a file, I get the same message as above but the file is saved as well.

Can somebody tell me how I can solve this problem.

Kind regards
Gerard
1 REPLY

Re: Error message

Esteemed Contributor
Esteemed Contributor
Possibly re-install. Is it installed on your C:? Was UAC turned off and the install ran using the "Run As Administrator" selection?


Ken

Production: ST10 MP3
Testing: SE 2019