Error starting 2D ST7

Creator
Creator

When I start free 2D ST7 (new installation) I get an error message: system clock has been set back, that is not the case I have checked in my bios. What to do?

3 REPLIES

Re: Error starting 2D ST7

Esteemed Contributor
Esteemed Contributor

Not sure, but the message to the lower right of screen is interesting.  Smiley LOL

 

Capture.PNG

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP3] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Error starting 2D ST7

Siemens Phenom Siemens Phenom
Siemens Phenom

This is not an issue with the software. It is a system problem. The current license for Solid Edge 2D Drafting is a timed license. License updates are provided yearly for continued use and to help promote new versions of the softwarer. Because it is a timed license, there are checks made to ensure the license cannot be overridden. It would appear that the date of the machine has been at some point changed. Because of this system files will have future dates. The licensing mechanism checks for this and invalidates the license if there are system files with modified dates in the future. From a software standpoint there is nothing that can be done.

 

Regards,

Rick B.

Re: Error starting 2D ST7

Creator
Creator

Thanks Rick.