Extraction failed, file is corrupt

Experimenter
Experimenter

Downloads 99% real quick & then hangs on the last 1% for ever. Tried to download a number of times, all with the same result. Where do you get a download for ST6 thats not corrupt ?.

2 REPLIES

Re: Extraction failed, file is corrupt

Esteemed Contributor
Esteemed Contributor

Hi there,

 

The file is most likely corrupt because it wasn't completely downloaded....connection interuptions along the way are the most common cause.

I would recommend using one of the download managers available free online, and try again.

[one such example... http://www.freedownloadmanager.org/download.htm]

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP2] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Extraction failed, file is corrupt

Esteemed Contributor
Esteemed Contributor

Be aware that Siemens has changed a policy on download managers and now only supports "GetRight" a paid product and "DownThemAll" a FireFox only free product.  If you use another download manager and it misbehaves with too many connection attempts, you may get blocked.


Thanks,
Ken

Production: ST9 MP10
Testing: ST10 MP3