Reply

Fails to start


Just downloaded Solid Edge 2D Drafting, Version: 19.00.00.66, Date: 25-Sep-2006.
It loads splash screen then loads half the GUI for ~1 sec and then vanishes.
Licence file installed as per email instructions.
I have IE 6 and .Net, 1/2GB ram and 1Gb page file but it is a Pentium M 2GHz laptop.
Is that compatible?
Thanks. Looking forward to the test drive.
Richard.
1 REPLY

Re: Fails to start


Richard,
This sounds like it may be a graphics card issue. What type of graphisc card are
you using>
Rick B.