Groups and constraints

N/A

Is there a way to apply a constraint to an element in a group and have the group
follow the constrained element? Specifically, I want to align a group I have drawn
in a top view with its counterpart in the front view by applying the collinear constraint
to the two right edges. When I try this, I get inconvenient results: either the
edge alone moves in the top view, or the edge in the front view moves instead.
John
John Hilgenberg
2 REPLIES

Re: Groups and constraints

N/A
John,
Groups are a way to create a collection of objects. Constraints will still
work on the elements of the group separately. If you want a collection of
objects that cannot be changed outside of the collection, such as a pocket
on the face of a part, create a rigid set. Rigid Set is one of the
constraint commands. A rigid set fixes the geometry in the set so that it
cannot be modified outside of the set. You can then create a colinear
constraint of one of the lines in the set to a line outside the set and all
geometry in the set will move accordingly.
Regards,
Rick B.

Re: Groups and constraints

N/A

Thanks, Rick. I had never noticed that feature before. It's a little fussy the
way it shuns offsets, dimensions, etc., but once I understood the rules, it worked!
Regards,
John
-------------------------------
"Ricky Black" wrote:
>John,
>Groups are a way to create a collection of objects. Constraints will still
>
>work on the elements of the group separately. If you want a collection of
>
>objects that cannot be changed outside of the collection, such as a pocket
>
>on the face of a part, create a rigid set. Rigid Set is one of the
>constraint commands. A rigid set fixes the geometry in the set so that it
>
>cannot be modified outside of the set. You can then create a colinear
>constraint of one of the lines in the set to a line outside the set and all
>
>geometry in the set will move accordingly.
>
>Regards,
>Rick B.
>
>

John Hilgenberg