Reply

HOW TO FLIP THE DIMENSION TEXT


I've dimensioned an element and later added some more dimensions. Sometimes the
text will face one direction and other times the opposite direction. Is there a
simple way to make all the dimension text, say in vertical dimensions, face or be
read from the same direction?
Thanks,
Ron
Ronald W Latour
1 REPLY

Re: HOW TO FLIP THE DIMENSION TEXT

[ Edited ]
Ron,
Typically, text is read from the bottom followed by from the right.
That means text is upright. If vertical it will be read with the bottom of
the text to the right.
In the attached example, the two angled dimensions are read from the bottom.
Regards,
Rick B.