Reply

Help! Solid Edge 2D installs but will not run


Help Please!
I have SE2d installed but when I attempt to run the software the SE splash screen
comes up then the SE appears to be loading but then the software shuts down. The
window just dissapears. I get no error messages. When checking Task Manager there
is no sign of SE in the Aplications or Processes tabs.
I have just swapped out motherboards and freshly installed XP Home running on AMD
Athlon XP 2800. I had the same behavior on the previous motherboard and thought
I could have had a bad XP install but now I'm completely stumped. I have also tried
redownloading th file and a fresh install to no avail.
3 REPLIES

Re: Help! Solid Edge 2D installs but will not run


What type of graphic card are you using?

Re: Help! Solid Edge 2D installs but will not run


"Ricky Black" wrote:
>
>What type of graphic card are you using?

Thanks for the response. Im running a Nvidia GeForce FX 5200. Was wondering myself
if this could be the problem and apologize for omitting the video card from my system
specs in the original post.

Re: Help! Solid Edge 2D installs but will not run


Don,
Here are a few things to try.
Clean up your temp directory.
Ensure you have enough page file size. Typically you want about 2 times the RAM.
Disable the hardware acceleration on the graphics card. If this works, you can start
moving it back up to find the best setting.