Reply

Hexagon


Good afternoon, how does one draw hexagon, octogon, etc in Solid Edge 2d?
2 REPLIES

Re: Hexagon

Hendrik,
Currently there is not a specific command to create an N-sided polygon. You
can create a closed region and use the equal conctraint to set the lengths
of the sides to be the same. Then set the angles between adjacent edges to
be the same.
Regards,
Rick B.

Re: Hexagon

I would add that there is a supplied VB macro to create n-sided polygons,
but it only supplied/works with the maintenanced version of Solid Edge 2D as
well as the full 3D version.
--
Ken
http://grundey.blogspot.com
"Ricky Black" wrote in message
news:461cfa0a$1@bbsnotes.ugs.com...
> Hendrik,
> Currently there is not a specific command to create an N-sided polygon.
> You can create a closed region and use the equal conctraint to set the
> lengths of the sides to be the same. Then set the angles between adjacent
> edges to be the same.
>
> Regards,
> Rick B.
>