Reply

IF 2D DRAFTING FAILS TO INSTALL - READ THIS

If 2D Drafting fails to install and gives an error about a '.tmp' file
cannot be found, there is a fix for the problem.
Go to the following web site and install .NET 3.5. This is a Microsoft
install.
http://www.microsoft.com/downloads/details.aspx?familyid=333325FD-AE52-4E35-B531-508D977D32A6&displa...
Simply click on the Download button on this web page.
I prefer saving the file to a specific location and then running the file
from there.
After you have installed .NET 3.5, install Solid Edge 2D Drafting again.
Regards,
Rick B.

9 REPLIES

Re: IF 2D DRAFTING FAILS TO INSTALL - READ THIS

Works, thanks

Re: IF 2D DRAFTING FAILS TO INSTALL - READ THIS

It helps in installation. But it doesnot open for me. When I try to open, pop up opens asking me to "run" it. And again it goes through same process of intallation. I am confused. Please Help.

Re: IF 2D DRAFTING FAILS TO INSTALL - READ THIS

The executable you downloaded is an installation executable only.
You do not run the download executable to run the software.
At this point have you successfully installed the software?
If you have, there will be an entry unser 'Start-All Programs' for Solid
Edge 2D Drafting.
This is where you run the software.
Regards,
Rick B.

Re: IF 2D DRAFTING FAILS TO INSTALL - READ THIS

Thanks! This solved my installation problem.
Peace, TAZ

Re: IF 2D DRAFTING FAILS TO INSTALL - READ THIS

Hi, ive just tried to install the solid edge software, and i get a messge saying:
" The SSE2 instruction set is not supported by this cpu, solid edge ST2 does not support processors that don't include the SSE2 instruction set. Instalation will terminate"

Any ideas on how i can get this to work, or do i need to upgrade my system?

Re: IF 2D DRAFTING FAILS TO INSTALL - READ THIS

Am 01.06.2010 19:33, schrieb jeremyb1929@live.com:
> Any ideas on how i can get this to work, or do i need to upgrade my
> system?

maybe you can update your processor.
http://en.wikipedia.org/wiki/Streaming_SIMD_Extensions
http://en.wikipedia.org/wiki/Streaming_SIMD_Extensions#Later_versions
regards

Re: IF 2D DRAFTING FAILS TO INSTALL - READ THIS

Am 01.06.2010 19:33, schrieb jeremyb1929@live.com:
> Any ideas on how i can get this to work, or do i need to upgrade my
> system?


maybe you can update your processor.

http://en.wikipedia.org/wiki/Streaming_SIMD_Extensions
http://en.wikipedia.org/wiki/Streaming_SIMD_Extensions#Later_versions

regards



Lol, i would'nt even know where to begin, guess i will have to try and buy a new system

Re: IF 2D DRAFTING FAILS TO INSTALL - READ THIS

Am 04.06.2010 15:34, schrieb jeremyb1929@live.com:
> ...
> Lol, i would'nt even know where to begin, guess i will have to try and
> buy a new system
>

some older porcessors are able to update to SSE2. anyway.

the new system ...
>http://www.plm.automation.siemens.com/en_us/products/velocity/solidedge/overview/system_requirements...
regards

Re: IF 2D DRAFTING FAILS TO INSTALL - READ THIS

If 2D Drafting fails to install and gives an error about a '.tmp' file
cannot be found, there is a fix for the problem.
Go to the following web site and install .NET 3.5. This is a Microsoft
install.


I would appreciate this info to appear in System Requirements section on Free2D product page. http://www.plm.automation.siemens.com/en_us/products/velocity/solidedge/free2d/index.shtml

"Software Requirements: Windows XP with Microsoft .NET 2.0 updated to SP1 (Microsoft KB945757)."

IMO, Microsoft KB945757 hotfix should be referred instead of .NET 3.5, since software setup for individual companies will require stable environment on versions.


Thanks for the community for great support!