Reply

Import AC1015

Hello,
i try to import a dwg, drawed with atuocad 1015.
i always get it in with scale 1:300.
The scale 1:300 was set in autocad
a lenght of a line in the 2Dmodell area are not (for example) 300 mm,
ist 1 mm. Iam faild with all i have tried.
regards
Robert
2 REPLIES

Re: Import AC1015

Robert,
There is not an option to scale durong Open.
You do have options for Inch or metric.
Make sure you use the correct inch or metric template.
If this is really a scale problem other than insh and mm,
you can use the scale command to scale the geometry after you open the file.
It is on the drop list under the Mirror command.
When you run the Scale command, press CTRL+A on your keyboard.
This will select all geometry for scaling.
Regards,
Rick B.

Re: Import AC1015

Am 25.02.2011 16:49, schrieb Ricky Black:
> ...
> If this is really a scale problem

jes, ist was.

> other than insh and mm,
> you can use the scale command to scale the geometry after you open the file.
> It is on the drop list under the Mirror command.
> When you run the Scale command, press CTRL+A on your keyboard.
> This will select all geometry for scaling.

Thanks a lot.
Robert